This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5012: 大占空比工况下,空载电流较大

Part Number: LM5012


使用LM5012/5013,设计36Vin转33Vo输出,空载工况下,系统未进入sleep 模式,空载电流大于0.8mA

器件参数:Ron=330kΩ,电感L=100uH,  Ca=3300pF,Ra=220k~510k,Rb=47pF~100pF,Cout = 10*2uF

橙色:48Vin转33Vo,空载下Vsw波形,I空=80uA,正常进入sleep模式

白色:36Vin转33Vo,空载下Vsw波形,I空≈800uA,周期异常,Ton大于设定时间,空载电流大

空载电流异常时,Vsw打脉冲的周期明显小于正常工况下

需求调试方案?调试方向?

  • Hi

        建议建议你借助芯片官网的在线仿真webench确认一下。

       其次确认一下芯片,很多静态电流异常都是芯片的问题。

       最后就是测试,单独给FB 1.5V电压看看静态电流是否正常? 如果正常反馈,静态电流是mA级别是偏大的。