This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: 能否替代BQ25723使用

Part Number: BQ25792
Other Parts Discussed in Thread: TPS65987D, BQ25723

各位工程师你们好:

我原来使用TPS65987D+BQ25723做了一套充电电路,但这个组合无法用外部LED灯指示充电状态。

原来设计是使用TPS65987D获取PD协议供电,然后987D的I2C配置BQ25723充电电压/电流

设计条件是:通过987D控制,到BQ最大供电20V/3A,最小5V/1A;电池充电电压8.7V,最大充电电流5A.

现在保持使用987D快充协议芯片不变条件下,

计划用BQ25792替换BQ25723,使用792的VIN2做输入,请问能否进行替代?

或者有没有其他能有STAT状态输出的升降压BQ充电芯片推荐。

谢谢!