This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43060: TPS43060 不同输入电压,待机电流相差较大

Part Number: TPS43060


使用TPS43060 做的BOOST电路

输入9-17V  输出  24V  5A  频率设定500Khz,电感量3.3uh,原理图参考的是828a

空载待机  9-12.5V    电流60mA

                     13V      电流23mA

                     14V      电流小于1mA

是什么原因导致输入待机电流变化

 

  • Hi

        输入电压越小,电流消耗越大是正常的,但是看起来达到60mA是有些偏大的,一般这类外置MOS的电源方案,电流消耗mA级别是正常的。

        建议你选择Qg尽量小的MOS, 其次频率可以适当降低也可以减小静态输入电流。