This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62864: 输出疑问

Part Number: TPS62864

Vin=3.7V,Vout=0.75V,Cin=2*10uF   Cout=2*22uF   L=0.24uH

电路采用典型电路,如下所示,现在负载端的电流瞬态是0.9A/100nS,Imax=1A;想请教下,在这个瞬态条件下,芯片输出端的电压跌落/输出电压响应是什么样的?这个有相关的仿真或者是实际测试结果支撑吗?