This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200: How to determine the withstand voltage value of the output capacitor?

Part Number: TPS92200

VIN=9VDC

Output Voltage=2.9VDC(2.8+0.1)

R1=430mΩ

How to calculate the withstand voltage value of C4?

Is the withstand voltage value of 25VDC for C4 sufficient?