Other Parts Discussed in Thread: BQ28Z610,
您好!我们使用BQ25798给系统供电并给电池(2芯,BQ28Z610)供电时,当电池温度在充放电保护温度点附近会发生系统重启或关机一次,并且这个重启或关机问题发生随着电池温度保护点设置改变而改变;(我们现在设置为0°,则当电池温度为0°时,会概率出现一次重启或关机,设置为-5°,则问题发生在-5°,如图为电池电量计充放电温度设置);我们现在解决这个问题是需要将BQ25798的TS ignore(设置0x18 bit0=1)才好,但我们实际设计使用了TS功能,不希望忽略它;请问能帮忙解释下吗?究竟是哪里有问题呢?怎么排查?如下是我们的原理图,TS脚上的NTC在电池pack上,是一个类似103AT的NTC;