-
SRP SRN这个口的耐压是多少,规格书说的情况很多,有点儿不清晰,我想知道我测电流时,多少V的模拟量会使这两个pin坏掉?因为有时候会出现短路或者过流的情况,或者供电或基准电压复位等等。如果SRP对SRN的电压超过+-200mV,但是SRP,SRN分别对地没超过max值呢?比如说SRP-SRN电压为500mV的情况,这两个pin会损坏吗,或者其他pin损坏
-
VSCD这个值是什么意思?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您对TI产品的关注!
关于你的咨询,BQ76952的SRP和SRN引脚的绝对定格电压是一个相对值。
Min VSS–0.3 to Max VREG18 + 0.3
与VSS和 VREG18的值有关联。
例如: VSS是0V, Vreg 18是typ.值1.8V。
那这两个引脚的耐压就是 -0.3 to 2.1V
推荐的输入电压范围,在datasheet有明确的说明。
有2种情况,你测电流时推荐的范围是±200mV.
VSCD是设置放电电压短路阈值的,对应很多设定范围。
如何设定,你可以参考datasheet中的这个例子。
Considering a short circuit discharge current of 80 A, the recommended maximum SRP, SRN
voltage of ≈0.75 V, and the maximum SCD threshold of 500 mV, the sense resister should be below
500 mV / 80 A= 6.25 mΩ maximum.
希望我的回答对你有所帮助。