Hi!
我最近使用UCC28070A芯片设计了一个PFC电路,输入电压为85~276V,参考了SLUA479B的设计。
设计输出功率为2500W,但是检测电路输入电流波形过零点处异常,出现一个平台,且随着负载增大而变化。请帮助我排查问题,谢谢!
输出功率为300W,输出电压为395V。
输出功率为700W 电压为395V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.