This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: 0%电量电池在主机端放置3周后开机电量显示100%

Part Number: BQ28Z610

TI 工程师你们好!

     我们有一个使用BQ28Z610电量计的2S1P 5000mAh电池组,出厂前已按流程成功进行电池容量学习,然后送到客户处进行测试,发现以下问题:

     发现1pcs充满电的电池组在主机上放电(放电功率约2.5W)至0%电量后关机,放置3周后主机开机显示电池电量100%;此时将电池与主机断开再重新连接后,主机显示0%电量,请问是什么原因可能导致的电量跳变?

     补充电池与客户主机的相关信息:

     1.附件为BQ28Z610 学习前的GG文件;XZ-GSP806090-2S1P-V1_BQ28Z610_2023-10-16.gg.csv

     2.电池I2C信号线直接连接到主机MCU,通讯线上也有10k的上拉电阻。MCU由电池供电,电压为3.3V,电池和MCU共用一个地;

     3.在主机正常使用状态下没有发现电量百分比有跳变;

     4.主机在电池0%时开机,大约2.7A峰值持续1ms,然后持续650mA。