This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: 关于set>configuration>power config寄存器配置问题

Part Number: BQ40Z50-R2


hi,你好!

我在配置power config这个寄存器的时候有一些疑问,bit9和bit8在技术手册种没有更多的描述。有这个2个疑惑:1、[SLEEPWKCHG]不使能充电还能唤醒电量计不?和Power>Wake Comparator的设置有什么区别;2、[SLP_ACCUM]这个休眠模式的积分是用来处理什么情况?

SLEEPWKCHG (Bit 9): Enables the sleep wake charge feature
1 = Enables sleep wake charge feature
0 = Disables sleep wake charge feature
SLP_ACCUM (Bit 8): Enables charge accumulation while in SLEEP mode
1 = Enables charge accumulation in SLEEP mode
0 = Disables charge accumulation in SLEEP mode