This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940

Other Parts Discussed in Thread: BQ76940, BQ78350, EV2400

1.BQ76940 ADC偏移量和系数都是从寄存器读取而成,假设每个76940的偏移量和系数都不一样的话,对于相同的程序而言,设置OU_TRIP、UV_TRIP寄存器的值是一样的吗,那么每个BQ76940的过压和欠压设置值不是不一样的吗,会不会差距很大?

2.78350 FIRMWARE,我看datasheet配置说需要下载FIRMWARE才能使BQ78350正常工作,而TI官网该链接有问题,打不开,能否给个下载链接?

3.单独使用EV2400时,IIC的SDA、SCL对GND的电压均为4.1V,导致BQ76940与EV2400无法正常通信,能否有办法解决?

  • 1. OV 和UV的保护是依据内部独立的比较器来设定的, 精度和ADC采样的精度无关

    2. http://www.ti.com/lit/zip/sluc572 是可以下载的

    3. 在不接bq76940的情况下,测量ev2400的i2C上也是有4.1V的电压?

  • 1.对于程序而言,寄存器OV_TRIP、UV_TRIP设置的值都是一样的,我的意思是GAIN和OFFSET的值因为是读取的,每个片子的值一样吗,要是不一样,不是就会导致OV和UV的值不一样?

    2.之前我点过那个链接,中文界面和英文界面都下载不下来

    3.是的,USB插拔也试过,电平仍然4.1V,每次都要等几个小时电平变成3.1V左右,也不知道什么原因。