This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76200: CHG,PCHG,DSG 不受控,直接输出VBAT

Part Number: BQ76200


这是14串电池原理图,67200直接驱动MOS管,MOS管并联,充电10个,放电10个,还有一个预充电

现在的问题是,芯片上电后,使能信号都为低电平,但是CHG,PCHG,DSG直接输出了电池电压BAT,即59.5V,1.输出信号CHG等的高电平就是BAT电压吗,2.看真值表,使能低电平,输出也应该是低电平,但是输出是高电平,是不是可以判定芯片损坏了,3.电池电压BAT最高可以到60.2V,选型有问题没,或者您这里有推荐的.4.原理图您看有没有明显的错误,麻烦提点建议

另外单测76200,不接MOS管,只供电,使能都为低电平,结果输出信号也是高电平——还是BAT电压。