This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: 重复充放电数次后,电量百分比不更新

Part Number: BQ27520-G4


我们正在使用bq27520-g4电量计芯片,电池标称电压3.7V,容量3500mAh;

在充放电的测试过程中,电量百分比 能随着电池充放电变化,从0%~100%,再从100%~0%;

重复充放电数次之后,电量百分比卡在100%不更新,如下图,我们将电池从4.1V放电到3.75V左右,电量始终为100%无变化;

请问这种现象可能是什么原因造成的,电量计当前状态是否正常?