This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61094: 我需要一款用于锂电池输入,给超级电容充电的电源芯片,请帮我推荐一下;

Part Number: TPS61094
Other Parts Discussed in Thread: TPS61220, TPS63802, TPS61022, , BQ25173, BQ25703A

芯片需求:锂电池2.6~4.2V的电压输入,超级电容工作电压最好也可以限制在该范围内,最好是可调版本输出,另外在超级电容后端会接入稳压模块以及负载,稳压3.3模块选用的是TPS61220;后端负载至少需要电流400mA(电压在3.3V情况下);以下是整体的构型:相当于我需要连接锂电池和超级电容的一款单项DCDC芯片。请帮我推荐一款在尺寸上、静态电流以及效率上较为均衡的芯片。

Chip requirements: lithium battery 2.6 ~ 4.2V voltage input, supercapacitor operating voltage can also be limited to the range of the best, preferably adjustable version of the output, in addition to the back end of the supercapacitor will be accessed in the voltage regulator module as well as the load, the voltage regulator 3.3 module selection is TPS61220; the back-end load at least need to have a current of 400mA (voltage in the case of 3.3V); the following is the overall configuration This is equivalent to a single DCDC chip that I need to connect to a Li-ion battery and a supercapacitor. Please help me recommend a chip that is more balanced in terms of size, quiescent current, and efficiency.

  • 感谢您对TI产品的关注!
    关于你的咨询,你看看这个TPS63802 buck-boost converter 应用于Supercapacitor的芯片。
    我看参数适合你的应用。
    www.ti.com/.../TPS63802

  • 感谢回复!已经在考虑该芯片,还想请问下您,关于贵公司是否有更适合于超级电容充电用芯片,我所查询到的

    TPS61094;TPS61022是否可用,另外,注意到贵公司有BQ系列芯片,例如

    BQ25703A;BQ25173;

    是否能够帮忙介绍一下这几款产品,哪款更加适合我的应用需求~

  • TPS63802 是单纯的buck-boost converter转换。

    TPS61094;TPS61022不太适合。

    而BQ25703A;BQ25173也是可以接Supercapacitor的芯片。

    BQ25703A带I2C控制,BQ25173带CE控制pin。

    相对于TPS63802 简单的电压控制转换。我认为BQ25703A和BQ25173这种充电控制芯片更智能些,更加适合你的应用。

    你可以尝试申请下样片,评估选择哪款芯片更适合你。

    芯片主页>Ordering & quality> 点击request sample

  • 感谢,我去查看了BQ25703A和BQ25173的数据手册,似乎输入电压有点高了,尤其在典型中,输入电压已经超出了我们所选用锂电池2.6~4.2V的工作区间,因此我们只好考虑其他芯片。

    另外TPS61094在手册中介绍是双向DC,貌似是超电能提供输入,给不是给超电充电。您是否可以解答一下TPS61022不适用的原因。

    另外因为我们考虑选一款比较适合给超级电容充电的芯片,但是在TPS61022数据手册中所提到的应用只是升降压,因此我们不能够确保适用性~

  • 你的设计是input范围既有高于ouput电压的,也有低于output电压的。

    所以buck-boost比较适合,TPS61022是boost,单纯升压。

    另外,你的框图我感觉supercap是备用电源吧,Battery charger ICs可能更适合。

    下面是所有的支持supercap的充电ICs。

    你根据参数自行筛选下。

    www.ti.com/.../products.html

  • 好的,感谢您的帮助,我们目前优先考虑您提到的BQ25173芯片,但是有一点我们担心的是在数据手册中提到输入电压最低为3.0V,我们采用的锂电池工作范围刚好为3.0~4.2V,这样会不会存在输出能力降低的情况,虽然锂电池也未必能够完全放电至3.0V以下。另外,我们在数据手册中注意到,所推荐的典型应用电路所描述的输入电压至少在5V以上,这让我们对于这款芯片是否还可用存疑。

    我们已经设计了一种给超级电容充电,充电电流为500mA,输出为3.6V的方案,请您帮忙看一下是否还存在问题。其中,HOST引脚是否可以直接连接芯片的输入保证持续给超级电容充电,而状态检测引脚的Vref电压是否可以直接连接芯片输出Vcs(这里我们暂时接了0Ω电阻保证可断开性)。

    我们也按照所提供的layout信息进行了PCB布局,如果以上均无问题,我们将考虑制版生产以及器件购买~

  • BQ25173是满足3~18V input应用的,推荐电路是典型应用,你也可以使用在3Vinput,满足范围就行。


    至于是否存在输出能力不足的情况,最好自己实际验证下。
    CEpin当低电平时,启用充电。
    STAT仅仅是状态指示引脚,输出能力弱,不建议接VCS。

  • 感谢感谢,如果STAT不接在输出电压上,那我应该接在哪里,这个Vref应该指的是一个参考电压,我应该如何处理这个Vref呢~

  • 我们评估板接的3.3V

  • 需要BQ系列型号吗

  • 目前在尝试使用BQ25173