LP8556的Datasheet中写明“Up to 50 mA Per Channel”,但是在Datasheet中的Device Options表格中“MAXIMUM LED CURRENT”中都是25mA或者20mA。
http://www.ti.com/lit/ds/snvs871h/snvs871h.pdf
这两者之间是否有矛盾之处,谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LP8556的Datasheet中写明“Up to 50 mA Per Channel”,但是在Datasheet中的Device Options表格中“MAXIMUM LED CURRENT”中都是25mA或者20mA。
http://www.ti.com/lit/ds/snvs871h/snvs871h.pdf
这两者之间是否有矛盾之处,谢谢~
您好,不矛盾。
芯片最终能到多少电流,跟散热条件有关系。芯片内部的current sink可以达到50mA的驱动电流,20mA测试是因为很多pannel的LED是20mA的,属于典型应用。
我是否可以理解如果PCB layout没有问题,任意型号的LP8556的6路led输出可以长时间同时承受50mA的sink current?
谢谢~