This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515HV: 请帮忙review 下原理图。谢谢!

Part Number: TPS92515HV


Dears,

     请帮忙review 下原理图,谢谢!

     客户设计指标是:输入兼容24V和48V 输入,输出700mA。

     之前调试中有发现了一些问题,主要是输出电流稳定性差,在18V 是一个分界线,18V 以上输出电流在不到700mA,18V 以下基本上在720mA,整个输出范围内电流一致性不好。而且输出在4V 以下时电流会急剧下降。另外在调光时LED 会闪烁,调完光后就正常了。

2783.G2M DC48-30Schematic Prints.pdf