This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2661-3-4EVAL: LM2661转负压30V

Part Number: LM2661-3-4EVAL


TI的专家,您好!

          我们现在需要一个5V(或者12V)输入,输出为-30V,电流大于100mA的电源芯片,请问贵司的LM2661是否可以实现该功能。

如不能实现,请推荐一个可实现的芯片方案,谢谢!