This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV743P: 應用在Body camera上 for CMOS 供電 Noise問題

Part Number: TLV743P

Hi all,

應用在Body camera上 for CMOS 供電,建議用料

目前使用了TLV74033& TLV74333PDQNR進行測試

RD進行了實驗如下: 

相同系統架構去更換TLV740與TLV743,Vin=3.63 or 3.36 or3.3V , Vout=3.3V 去做輸出影像實驗結果,

發現TLV743比TLV740 Source壓降多0.07V,Ripple沒有實際測量,但以最後影像品質來看,TLV743的效果比較差。

 

對於TLV740 vs TLV743有3個問題

  1. 為何TLV743比TLV740消耗更多能量?  這邊測得同個源頭電壓TLV743會比TLV740低0.07V
  2. 對於Vout=3.3V F=1Mhz Iout=100mA PSRR是否TLV740比TLV743更好? 是否有推薦更好的PSRR的LDO?
  3. 另外TLV740與TLV743的設計對於低於drop voltage的電源會如何操作?  E.q. : Vout 需要3V 但Vin=3.3V or以下,這樣Vout會有什麼問題? PSRR會如何