您好 我是用LMR16020设计了一款降压电路
按照webbench中计算的参数 该电路输入24V输出12V
但是实际测试中发现该电路不能正常工作,输出电压只有0.7V
已经测试将使能引脚悬空,按照评估版手册接入分压电阻(4.5v)
或者是EN脚接入VCC 该电路都不能正常工作
请问我该如何修改
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你将R1换成45Kohm,L1换成15uH看下,如果还不好用。
我们是怀疑你PCB设计有问题,那你对照下TI评估板的设计电路和PCB layout自行排查下原因。
www.ti.com/.../snvu497
gerber files。
e2e.ti.com/.../SV601284A_2D00_GerberMin.zip