This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR43620-Q1: 偶发输出失控(过压)问题

Part Number: LMR43620-Q1

器件型号:LMR43620MB5RPER

使用环境及问题:作为12V转5V的DCDC使用。绝大多数情况下工作正常,输出稳定且纹波很小。但在极个别情况下5V输出会失控,趋近12V。这种情况发生概率很低,目前还没有摸清触发条件。但是目前碰到的所有过压情况都是一上电输出就过压,还没有出现正常输出期间电压升高过压的情况。并且一旦出现输出过压,即使把输出手动短路后再恢复,输出电压恢复后仍旧过高,只有断开输入电源重新上电才能恢复正常输出电压。请帮忙看一下问题原因,谢谢!

原理图:


Layout:

出现输出过压故障期间各个引脚测量结果:
Vin (Pin 4): 12.023V
Vout (应为5V): 11.893V
Vfb (Pin 8): 2.316V
Vpgood (Pin 2): 0.0541V
Vcc (Pin 7): 3.273V

出现过压问题时SW(Pin 5)引脚波形:

出现过压问题时SW(Pin 5)引脚波形(局部放大):