This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: PMID与SYS为后续系统供电的疑问

Part Number: BQ25798
Other Parts Discussed in Thread: BQ24610, , BQ25895

Hi,

我以前使用BQ24610芯片,现在尝试使用BQ25798芯片,存在一些关于PMID与SYS的疑问:

假设VBUS端口输入20V,电池端口配备了4节锂电池且电压为16V,令D+与D-引脚悬空,此时电池处于充满状态,后续我只有一个系统需要20V的供电。

  1. 此时后续系统应该接在SYS引脚后方还是PMID引脚后方?SYS引脚的输出电压与VBUS是相同的吗,那PMID呢?
  2. 如果VBUS端口的20V电压被移除,此时电池将为后续系统供电,SYS引脚的输出电压是电池的16V吗,那PMID呢?
  3. 我参考了关于BQ25895的一系列问题,了解到PMID和SYS可以同时输出,假设当VBUS供电5V时,PMID会输出5V,SYS会输出降压得到的3.5-4.5V;如果VBUS未供电,SYS会输出BAT的电压,PMID通过BAT升压至5V,BQ25798的性质是否与其类似?
  4. 在手册图10-2与图10-3中,我观察到只有Backup Mode被启用时,PMID后方才会有Uninterrupted Power Supply,是否代表着使用PMID为后续系统供电必须开启Backup Mode?Backup Mode的功能是当VBUS<VBAT时,由VBAT反向为VBUS充电吗?
  5. 在手册图10-2与图10-3中,这两幅图是完全一样的吗?Ship FET代表的是否是SDRV引脚后方的Optional NMOS,即在图10-3中,是否应该将Optional NMOS移除?