This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295: 关于芯片PMID电源供电切换问题

Part Number: BQ24295

尊敬的工程师

你们好。写这个贴主要是关于BQ24295这个芯片的使用问题,现在这颗芯片在控制上没什么问题,可通过IIC修改对应的寄存器值,对应其他使用是有些疑惑,

1.我在使用PMID输出的5V电源时发现当外部输入去除时PMID输出的5V会断电重新启动,我本来打算使用这个5v来驱动LCD显示器,拔掉电源输入黑屏重启显然是不对,所以想请教一下这个是正常的吗?还是这个芯片不合适。是否有合适的芯片推荐。

2.关于芯片TS引脚的问题。这个引脚是系统温度监测功能,如果不使用的是否使用电阻对这个引脚的电进行分压。我通过修改寄存器关闭温度功能好像就不充电了。

3.如果需要检测电池的电压是不是需要另外增加电池电压检测的电路。好像没有通过寄存器读取电池电压的功能。