This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940

1.BQ76940 ADC偏移量和系数都是从寄存器读取而成,假设每个76940的偏移量和系数都不一样的话,对于相同的程序而言,设置OU_TRIP、UV_TRIP寄存器的值是一样的吗,那么每个BQ76940的过压和欠压设置值不是不一样的吗,会不会差距很大?

2.78350 FIRMWARE,我看datasheet配置说需要下载FIRMWARE才能使BQ78350正常工作,而TI官网该链接有问题,打不开,能否给个下载链接?

3.单独使用EV2400时,IIC的SDA、SCL对GND的电压均为4.1V,导致BQ76940EV2400无法正常通信,能否有办法解决?

补充说明:

1.对于程序而言,寄存器OV_TRIP、UV_TRIP设置的值都是一样的,我的意思是GAIN和OFFSET的值因为是读取的,每个片子的值一样吗,要是不一样,不是就会导致OV和UV的值不一样?

2.之前我点过那个链接,中文界面和英文界面都下载不下来

3.是的,USB插拔也试过,电平仍然为4.1V,每次都要等几个小时电平变成3.1V左右。