Remove load then connect it. LP8866 will trigger error. And the output was turned off.
Can I reset LP8866, and trigger the output turn on without switch power?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您对TI产品的关注!
关于你的咨询,看你的描述,断开负载在连接,你应该是触发了Open LED Faults (OPEN_LED)。
你看下datasheet的7.3.9.3.1 Open LED Faults (OPEN_LED)章节。
But the LED_STATUS bit could be cleared by the interrupt clearing procedure.
7.5.2.2 Clearing Fault Interrupts
你对 LED_STATUS寄存器的STATUS bit and a CLEAR bit写入1,清除下fault。

如果后面负载是正常的,应该是会点亮,
如果新的LED fault被诊断出来,还是会报错。
The detail of open LED faults can be read from bits OPEN_LED and LEDx_FAULT (x = 1...6).
These bits maintain their value until device power-down.
But the LED_STATUS bit could be cleared by the interrupt clearing procedure.
If a new LED fault is detected, LED_STATUS is set and an interrupt generated again.
如果仍有问题,建议你直接问问这个芯片相关的设计工程师看看他们的建议。
TI国外的工程师,请使用英文咨询。
另外,英文论坛咨询需要使用公司后缀的邮箱。
您需要将MYTI账号中的免费邮箱更改为公司域名邮箱才能在E2E英文论坛发帖。
更改方法参阅这个帖子:e2e.ti.com/.../faq-how-do-i-change-the-email-address-in-my-profile