This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: 反向模式下SYS电压调节精度问题

Part Number: BQ25750


1.在测试自行设计的BQ25750样板时,使用可调电源在BAT端提供18V的输入,连接电子负载到SYS端口,打开反向模式并设置调节电压为24V,在较低电流下可以达到可以接受的电压精度,但在2A恒流负载模式下,SYS端输出电压已降至22.85V,偏离设定值24V过多;请问如何补偿这种压降?

2.设置反向模式电压为24V,在2A负载下无法冷启动反向模式,但在较低电流负载下可以冷启动并逐渐加载至2A(虽然仍存在问题1所述压降),该如何解决这个问题?