我有一款工业平板,由于某些限制导致电池是3S2P的锂电,适配器是19V,所以背光用TPS61176,Vin是来自易电源的5V输出.
后来更换高亮屏之后TPS61176的6个输出通道并联(6*35mA)不足以支持背光3S13P的需求(9V,500mA),考虑到buck的背光驱动不太适用于锂电单独工作的情况,但boost的驱动芯片又不好选择,比如TPS61199等高输出电流的芯片要求输入大于8V,需要前级再增加一个DCDC,请问用哪个芯片比较合适?如果用易电源的5V作为输入,TPS61169可以支持9V 500mA的输出吗?