This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62135: TPS621351输出电流波动。

Part Number: TPS62135

您好,我正在使用TPS621351。 我设置的FB是0.298V,反馈采用<使用TPS63xxx 降压升压转换器来驱动LED 的不同方法>第4条第4点提高LED电流控制精度,但是我发现我的输入电压波动,输出电流也会变化。 当输入电压低于11.14V时,输出电流为1.85A并开始下降。 我的测试环境是TPS621351 SS引脚接120K电阻下拉,VFB设置为0.298V,R1使用953K,R2使用80.6K,采样电阻为R150。我的DAC为0-3.3的PWM信号,PWM通过RC滤波(1uF+1K)输入到R1。我尝试更换电阻,结果是一样的。 输入电压跌破11.14V后,输出电流开始波动变小。 我怀疑这是占空比问题。 我将 TPS621351 的 MODE 设置为低电平,但没有强制 PWM。

希望得到有效答复,谢谢。