This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2492: 是否可以禁用功率保护功能?芯片是否具有容性负载缓启动功能?

Part Number: TPS2492


1.TPS2492具有功率限制功能,手册第八页写到If the constant power limit is not used, PROG should be tied to VREF through a 47-kΩ resistor,我的理解为可以在PROG和VREF间串联47k电阻以禁用功率保护功能。

实际中在PROG和 VREF间串联47k电阻并不能禁用功率保护功能,通过短接VCC和SENSE禁用,但VCC和SENSE短接后芯片又失去了电流保护。如果保留功率保护功能,在带载启动过程中会导致进入功率保护而烧管。

例如这张波形,蓝色是驱动Vgs,粉色是Vds电压,黄色是流过MOS的电流。有功率保护时,带载启动会烧毁。

想咨询是否可以禁用功率保护功能?或者怎样设计可避免带较大容性负载或带载启动的工况下烧管。谢谢。

 .

2.手册中提到可以通过通过CGD进行dV/dt控制,但我经过实测后感觉效果并不明显。想咨询dv/dt控制是否可作为负载缓启动使用?是否因为配置不当导致效果不明显。