This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920: BQ76920 电池电压精度问题

Part Number: BQ76920


客户使用BQ7692003 做4串电池BMS,现发现有部分电池电压采样与实际测试偏差较大,数据见附件。客户要求四节电池总压偏差在24mV以内,目前有24PCS超出范围为:26-49MV。

请帮忙看下该芯片的电压采样的最大误差范围是多少,还是批次不同导致该问题?

我从datasheet 上没有看到Vcell acc 的值,只有ADC 精度的值,在0-60度时是正负25mV,4节就是正负100mV,如果这个就是单节电池电压采样的精度的话,客户最大的49mV 偏差也是在datasheet 的允许范围内。

RDXD06 压差测试验证20240424.xls