HI TI
使用TPS54A20做buck电路,输入电压是12v,输出电压期望是3.3v@10A,电路如下,测试结果输出电压只有2.96v,但是即使我再调高R9=82K,输出电压反而是降低到了2.6V,请问是原因?另外,用万用表测试FB的电压时,电路就没有输出,即使是再次通电也是没再有输出,是不是这芯片有这个问题的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI
使用TPS54A20做buck电路,输入电压是12v,输出电压期望是3.3v@10A,电路如下,测试结果输出电压只有2.96v,但是即使我再调高R9=82K,输出电压反而是降低到了2.6V,请问是原因?另外,用万用表测试FB的电压时,电路就没有输出,即使是再次通电也是没再有输出,是不是这芯片有这个问题的?
刚再看了规格书:“……输出电压范围为 0.51V 至 2V,反馈基准电压为 ±0.5%……”,糟糕,已经是生产的了,请问是否有pin2pin的芯片替换?
您好
我帮您查了一下,很遗憾,没有pin2pin的。
比较相近的话,可以考虑这款,但是封装不同,需要改板,您可以看看。
TPS54020 data sheet, product information and support | TI.com
是得改板的了,请问TPS53319DQPR,是否合适作为这个应用?