This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54340-Q1: 输入电压临界时,输出状态不稳定

Part Number: TPS54340-Q1
Other Parts Discussed in Thread: TPS54340

Hi E2E:

我们的客户在使用TPS54340-Q1设计产品时遇到问题:

电源电路截图如下



产品工作的的逻辑:外部电源VBAT输入后通过TPS54340降压到5V,给MCU供电;

同时当IGN_ON(唤醒)输入给MCU检测到低电平时,MCU处理后级控制信号,激活后级LDO为SOC供3.3V,1.8V和1.15V供电,产品的各项功能开始正常工作。

我们遇到的问题是:

外部电源VBAT输入电压为4.3V~5.17V时,TPS54340彻底关断,没有输出;

当外部电源VBAT输入电压为5.17V~5.26VTPS54340处于不稳定状态,在不停的波动,输出电压在不停的拉高拉低。

        此时观察到整体的电流也在不停的波动;电源VBAT输入电压也被拉低;EN使能脚的电压也在不停波动。

输出电压波形:

En脚波形:

产品电流情况:



外部电源VBAT输入电压高于5.26V时,TPS54340能稳定的工作,输出稳定的电压5V,整个产品能正常工作。

请问输入电压介于5.17V~5.26V时,为什么会出现不稳定的状态?我们可以怎么消除这个状态,使得TPS54340要么处于彻底关断状态要么处于稳定输出?