This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: TVS selection for 24V battery system

Part Number: LM7480-Q1


Hi

Recently i use 74800 design for 24V battery system and start to select appropriate TVS for the enterance of the circuit.

I don't understand why choose TVS+ not based on clamp volatge instead of using breadown voltage which should be higher than 48-V jump start voltage, less than the absolute
maximum ratings of anode and enable pin of LM7480x-Q1 (70 V) and should withstand 65-V suppressed load
dump.

Wether we can choose one TVS+ for clamp voltage less than jump start then we can protest the backward circuit?

Looking forward to receive your reply soon

Thx

Panwen