Part Number: TPS54302
根据workbench设计的电路,5V转3.8的,如附件图片,FB测的参考电压只有0.45,导致输出只有2.8,芯片手册上提示参考电压0.6V吧,这是哪里有问题

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS54302
根据workbench设计的电路,5V转3.8的,如附件图片,FB测的参考电压只有0.45,导致输出只有2.8,芯片手册上提示参考电压0.6V吧,这是哪里有问题

您好
根据您所描述的情况,TPS54302芯片在将5V电压转换为3.8V时,反馈(FB)引脚测得的参考电压只有0.45V,而根据芯片手册,参考电压应为0.6V,这导致实际输出电压只有2.8V,而非预期的3.8V。以下是可能导致这一问题的原因和相应的解决步骤:
请您参考以上建议。