This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: TPS51200

Part Number: TPS51200

你好,工程师,

      我在使用TPS51200这款芯片为我的DDR3芯片提供电压。但是出现了一些问题。

1.经过测试。vin,EN的电压为3.3V,REFIN电压为0.75V,但是REFOUT、VO的电压都输出为1.413V(按照手册应该输出0.75V)。

2.当我将EN断路,即vin电压为3.3V,EN电压为0V,REFIN电压为0.75V。但是REFOUT输出为1.413V,vo输出为1.317V。(按照tps51200的手册,此时REFOUT输出应为0.75V,VO输出应为0,因为ENpin是disable的)。

请工程师为我解答以上现象的原因?是否是芯片出现了问题。以及REFOUT、VO两个引脚后续的电路是否会影响TPS51200的输出电压大小?