1. 输入48V转24V,电感15uH 强制PWM模式,频率140KHZ,输出24V在2~4A的时候,SW波形不正常,同时输出电压也不正常,在输出5A的时候又恢复正常。如下图:

请问下这属于什么情况?
2. SW频率调到1MHZ时,48V转24V,空载强制PWM模式,LM5149芯片温度很高,大概有七十多度,这个属于正常范围吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.