Other Parts Discussed in Thread: TPS82671
如果在固定25度情况下,Vin范围3.6~4V,EN=1.2,温度0-50℃情况下:
TPS82673:输出1.8V的ISD大概多少?
TPS82671:输出1.26V的ISD大概多少?
这个ISD主要受温度影响比较大还是输入电压范围影响较大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
目前我们这边只有数据手册中的典型值。
ISD随输入电压、温度和整个过程而变化, 都会造成影响。