hi IT
我用了webenchd 推荐的原理图做了TPS53319的电路,使用1.5uH和3.3uH电感,都没有3.3V输出,更换10uH电感就有3.3v输出,请问这是什么原因?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi IT
我用了webenchd 推荐的原理图做了TPS53319的电路,使用1.5uH和3.3uH电感,都没有3.3V输出,更换10uH电感就有3.3v输出,请问这是什么原因?

按照这个公式计算:【3/(14A*500KHz)】*{【(14V-3.3V)*3.3V]/14V}=4.285714285714286e-4*2.522142857142857=1.08uH,麻烦在确认下,感谢!
我这参照了评估板原理图,以及结合我的实际应用,在Vbst脚和Cbsst之间串联了3k电阻,把Rlbst改成了3k电阻,其他参数没有变。使用1.5uh电感是有3.3v输出了,但是带载电流只能是100mA,这和14A的要求相差太大了,当然我用的1.5A电感是14A规格的,因为我这个板急需生产,请问能不能给我个明确的解决方案,感激不尽!
这个芯片的电流输出是不是比例输出的,12v输入电压,始终调试不到带起14A?
感谢您对TI产品的关注!为更加有效地解决您的问题,我们建议您使用您的企业邮箱登录论坛并将问题发布在E2E英文技术论坛上(https://e2e.ti.com/p/addpost).