This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542EVM: BQ27542DRZR-G1低溫嚴重跳%

Part Number: BQ27542EVM


先使用乾淨的BQ27542參數,紀錄了以下數據:
1. 電池組在25度下充電,然後25度下使用2A放電,得到了數據:P28A 2A-3200mV rb 20240509 - 25oC
2. 電池組在25度下充電,然後放置到-30度2小時靜置,再使用2A放電,得到了數據:P28A-3200mV rb 20240508 - -30oC
上網Ti官網回報後得到rb數據,並且載入了gg file,但是發現一個問題,原本電池組的Qmax:5640mAh,被下修為:2811mAh,導致常溫下FCC顯示嚴重不足,因此手動修改Qmax,修改回:5400mAh後,做了以下兩個測試:

a. 在25度下,使用2.8A & 1A放電,得到了數據:P28A-3200mV rb 2.8A & 1A test at 25oC 20240514.log
b. 在-30度下,使用2A放電,得到了數據:P28A rb test - -30oC 20240515-fail
明顯可看到在25度下,2.8A & 1A放電都是很漂亮的,曲線都是正確。
但是溫度降為-30度後,FCC依然顯示錯誤的容量,2A放電後明顯跳%,直接27%跳到0%,雖然放電結束後FCC修正為3360 mAh(-30度下實際放出3540mAh),但是隨著溫度慢慢回升後,FCC又被強制回到了46xx mAh
請問是否有什麼設定需要變更?才能讓低溫曲線及FCC顯示正常