This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460-Q1: 环路稳定性测试判定规范

Part Number: LM61460-Q1
Other Parts Discussed in Thread: TPS54202

Hi,

     最近在做一个BUCK的环路稳定性测试,主要测的是伯德图,在测试过程对示波器参数的设置以及判断是否稳定的规范标准有些疑惑,特来请教一下。

我的应用输出电压是5V,输入电压9~16V,工作电流5A左右;

以下是我的问题点:

1、伯德图测试的起始频率和截止频率范围设置多少合适,我的开关频率设置的1938KHZ左右;

2、注入环路干扰的交变信号的幅值设置多少合适,我设置的50mV;

3、环路注入电阻的取值多少合适,我用的50欧姆;

4、穿越频率、增益裕度、相位裕度的判定规范标准是怎么定合理,能否给出具体的判定标准,这个标准其他BUCK的IC也能适用吗?我了解到规范的是穿越频率一般设置为开关频率的5~20%,增益裕度绝对值>12dB,相位裕度>45°;

劳烦帮忙解答一下,万分感谢!