This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43061: 升压后电压电流达不到预期问题

Part Number: TPS43061

你好,TI工程师,如上图:我目前设计了一款19.2~25.2V输入,36V10A输出的升压模块的原理图;现在板子遇到一下问题:

1、当24V输入时,输出电压是36.2V,负载仪从1A开始拉电流,最大输出电流只能达到1.8A。

2、当电流从1A到1.8A过程中,电压从36.2V慢慢降到32V左右。

3、当电流超过1.8A时,提供24V的稳压电源就开始出现类似于短路保护的状态;升压模块电感伴随着尖锐的呼啸声,同时能听到电感有咔哒咔哒声。

请帮忙分析下原因,这个电路原理图是在TI官网上仿真的结果,目前我这边没有解决问题的头绪,万分感谢!