This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
上面几个图是我设计的光源板的布线,VLED的供电电源是2.5V,最大电流5A,板子顶层跟底层都覆铜,SCL,SDA信号由另一个开发板提供
将板子焊出来后发现每个LED经过的电流到了190mA左右(我的R1到R5设置的阻值是180Ω,电流在100mA是正常),我尝试更换更大的电阻改变输出电流,换上510Ω的电阻,经过测量,流经LED的电流没有变化,还是200mA左右。
希望有大神给我解答一下,刚接触这方面,调试了好几天没有找到问题
这个是原理图