This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: 型号相当推荐

Part Number: TPS82130


请问TPS82130适用于电池供电类应用吗?该电源IC后面连接一个充电电容(3.3V),断电后因充电电容已充电,再启动担心大的突入电流对TPS82130有影响。

所以请问会有以上问题发生吗?

若TPS82130不合适,是否有带EN使能,同时能输出3.3V电压,输出电流能在4A以上,适合连接充电电容的DC-DC COVERTOR吗?

  • 您好

    TPS82130适用于电池供电类应用。这款电源管理IC(Integrated Circuit)由德州仪器(Texas Instruments)生产,专为电池供电的应用设计,具有高效率、低静态电流和宽输入电压范围等特点。

    关于您提到的连接充电电容(3.3V)后断电再启动可能产生的突入电流问题,TPS82130通常会包含软启动电路或相关机制来限制上电时的突入电流。这是为了防止电源启动时由于过大的电流而对电路中的其他元件造成损害。然而,具体的突入电流限制能力取决于TPS82130的设计和您所使用的具体电路配置。

    • Programmable soft start-up with tracking

    https://www.ti.com/lit/ds/symlink/tps82130.pdf

    详细细节请参考datasheet第9页有详细说明。