Part Number: BQ4050
4串磷酸铁锂电池 50Ah -- 300Ah ; 需要进行SOC计算;
请问以下两款芯片运用推荐哪款? BQ4050 和 BQ7692003
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
为了对4串磷酸铁锂电池(50Ah~300Ah)进行SOC(State of Charge,电量状态)计算,我们首先需要理解两款芯片的基本功能和特性:
BQ4050RSMR是德州仪器(TI)的电池管理芯片,它提供了完全集成的基于封装的解决方案,具有闪存可编程自定义精简指令集CPU(RISC),以及安全锂离子和锂聚合物电池组的保护和认证。它结合了超低功率、高速TI bqBMP处理器、高精度模拟测量功能、集成闪存、一系列外围设备和通信端口、N-CH FET驱动器和SHA-1身份验证,将响应者转换为完整的高性能电池管理解决方案。这款芯片适用于需要通过SMBus兼容接口进行通信的电池管理系统。
BQ7692003PWR也是TI的电池管理芯片,其设计考虑了低功耗,并支持3至5节的电池串联。该芯片支持锂离子、锂铁磷酸盐等多种电池化学物质,并且具有多种电池组管理功能,如监控(小区电压、电池组电流、电池组温度)、保护(控制充电/放电FET)以及平衡。这款芯片通过I2C接口与主机控制器通信,并集成了A/D转换器以实现关键系统参数的数字读数。
对于4串磷酸铁锂电池的SOC计算,两款芯片都具备一定的适用性,但选择哪一款需要根据具体的系统需求和设计要求来决定:
此外,还需要考虑参数datasheet和官方参考设计以及实际应用来进行慎重选择。