This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2378: 关于TPS2378的UVLO、VDD问题

Part Number: TPS2378

1.请问TPS2378的最低VDD能支持多少V,我这边POE级联到第六级后,第七级就不能正常供电了;每级产品功耗在3W左右,定级是AT class;

一级PD电压:51.27V

二级PD电压:48.26V

三级PD电压:48.26V

四级PD电压:43.16V

五级PD电压:41.25V

六级PD电压:37.83V

2.UVLO:

UVLO rising threshold:36.3~40V;

UVLO falling threshold:30.5~33.6V;

请问怎么理解欠压锁定这个值呢?