用LM5176做了一款9-36V输入,12V6A输出的模块,全电压范围上电可以正常输出12V,但输出带载能力随着输入电压降低会同步降低,最高36V电压输入带1A左右的电流后输出电压会降低到10V左右,之后再慢慢升高为12V,12V电压输入带0.3A左右的电流后输出电压会降低到5V左右并在小范围跳变,请问这是哪里出了问题,具体该怎么解决呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
使用LM5176设计的9-36V输入、12V6A输出的模块在带载能力上出现的问题,可能与LM5176的工作特性、电路设计以及外部组件的选择有关。以下是一些可能的原因及相应的解决方案:
https://www.ti.com/tool/WEBENCH-CIRCUIT-DESIGNER
这是官方的电源辅助设计工具,您可以将参数输入,工具可以给出相关参考设计。