This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下bq24650太阳能充电管理芯片的问题。

Other Parts Discussed in Thread: BQ24650

1.我发现BQ24650的demo板中vcc输入范围在5V-28V,但是BQ24650内部有一个6V LDO,给REGN和CE供电,假设Vcc输入在6V以下如5.5V,那么对HIDRV和LODRV有什么影响?对MOS管的开关影响大吗?请解释下原因。

  • 选用低驱动电平的MOS管,没什么影响,因为低驱动电平的MOS管,开启电压在3V以上基本就OK了。

  • 对于LDO,虽然不能工作在恒电流区 得到预定的正常输出电压,输出电流也很有限制。但看到LDO的输出作用是作为自举电容和低电平的驱动供电电压,如果这两者的电流都比较小的时候,即使没有预定的输出电压,但得到的输出电压也可能维持这两个模块正常的工作。