如题,寻求一款DCDC电源芯片
一、使用场景:
用在户外工作小车控制器上。
工作环境恶劣,昼夜温差大。
二、性能要求:
24V 电池供电,通过现寻的DCDC转换为12~15V输出,驱动无刷电机的MOS。
后级还需将12~15V转变为5V,供芯片使用。
5V的后级还会转变为3.3V,供MCU使用。
整个控制器控制部分电流不会超过500mA,主要就是供MCU、通讯芯片和MOS驱动使用。
三、概述
要求性能稳定可靠,抗干扰能力强,能满足户外恶劣环境。
求推荐,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.