This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776: 输出电压异常

Part Number: LM2776

设计思路是

  • LM2776输入电压为USB的+5V
  •  然后经过LM2776反向生成-5V 
  •  -5V电压接入TPS72325输出-2.5V

但是测试后 LM2776输出为-0.7V TPS72325输出为0.6V 导致运放无法工作

原理图如下

  

AGND和GND单点接地

TPS72325通过可控电源输入-5v 电流为4mA 

PCB:

想请问这样设计有问题嘛,如果需要改动有什么新的方案适合