This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A29: 出现关断闭锁故障

Part Number: TPS548A29


我使用TPS548A29来制作一个BUCK电源,实现12V/1V 10A的功能。

测试时使用电子负载,当输出电流上升时,输出电压会降低。当使用0.5Ω档位负载时,输出电压降为0.92V,2~3秒后器件关闭没有输出,只有当重新给EN脚3.3V电压时才会再次输出,但2~3秒后仍会闭锁关断。后增加VIN与VOUT电容仍有此问题。查阅datasheet发现闭锁关断的故障只会在OVP的情况下出现,深感困惑。

请问如何才能解决我现在的问题,感谢指正。

下面是我的原理图: