This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61027的参数计算

Other Parts Discussed in Thread: TPS61027

各位电源专家:

      我的一个基于电池的系统设计中,选用了TPS61027这个芯片。我们需求是输入2V~3V, 输出5V,电流50ma即可。swichpro和webench这两款电源设计软件中均没有该器件。

     我根据我的需求按照芯片手册中计算电感的方法进行了电感的计算,感觉明显不符合常理。计算出来的值很大。当然我可以依葫芦画瓢,按照参考设计选择6.8UH的电感进行设计,但是我还是希望能够知道L参数选择的依据。

   电感的计算我依据了数据手册中的公式(4)和(5)

  IL=50ma*5/(2*0.8)=156ma  。

 ripple我选择20%,开关频率为600K

  L =2*(5-2)/(156ma*0.2*600*5)=64.1UH   这个值明显不合理。

 

 恳请各位专家提供一下指导建议,谢谢。